Overview: Source block

Use this operation to import data from a source block. The source from which you import is the Architect Source block which will either be historical or real-time. This dataset can contain either discrete or continuous data. The various source blocks are:

  • Text source

  • Optimised database source

  • Tabular database source

  • Wonderware Historian source

  • Proficy historian source

  • PI historian source

  • OPC Classic Client source

  • OPC UA Client source

  • Discrete text source

  • Discrete optimised database source

  • Discrete tabular database source

  • Discrete Wonderware Historian source

  • Discrete Proficy historian source

  • Discrete PI historian source

  • Discrete OPC Classic Client source

You need to configure each of these source blocks, for example adding a timestamp field for continuous sources or selecting an index for discrete sources.

Properties

Category:

Import

Performance risk:

Potential high performance risk. The performance is influenced by the size of the text file being imported, which is determined by number of rows and/or the number of columns of the dataset.

Knowledge required:

Working knowledge of the software.

 

Effect on datasets

How many datasets are required to perform this operation?

None

Does it create a new dataset?

Yes

Can you reconfigure this operation?

Yes

Can you apply this operation to a locked dataset?

N/A

Does it modify the current dataset in any way?

N/A

Requirements

  • None

Results

  • A new dataset will be created.


Related topics:

  

CSense 2023- Last updated: June 24,2025